There are two options. The easiest one would be to send the OUTP? (@1) query. This will give you the current setting for the OUTPut command. The other way would be to send a STAT:OPER:COND? (@1) command. If bit 2 is asserted, then the output is off.
Applies to: N6700A, N6700B, N6701A, N6702A, N6705A, N6705B, N6710B, N6711A, N6712A, N6715A, N6715B, N6731B, N6732B, N6733B, N6734B, N6735B, N6736B, N6741B, N6742B, N6743B, N6744B, N6745B, N6746B, N6773A, N6774A, N6775A, N6776A, N6777A, N6751A, N6752A, N6753A, N6754A, N6755A, N6756A, N6761A, N6762A, N6763A, N6764A, N6765A, N6766A, N6781A, N6782A, N6783A, N6784A, N6785A, N6786A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |